GANTRY.PL.ERRFTHRESH

Description

This parameter sets the maximum position error. If the position error GANTRY.PL.ERR is larger than GANTRY.PL.ERRFTHRESH then the drive generates a fault. If GANTRY.PL.ERRFTHRESH is set to 0, the maximum position error is ignored.


  • Replace with note text.

Versions

Action Version Notes
Implemented 02-02-02-000  

General Information

Type Read/Write
Description Sets the maximum position error for Gantry Mode
Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range Depends on units. See Position Range for details.
Default Value

42949672960 counts


  • Default is adjusted to account for the units selected by the user.

Data Type Float
See Also AXIS#.PL.FB
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

GANTRY.PL.ERRFTHRESH

300eh

02h

Signed32

Position

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

GANTRY.PL.ERRFTHRESH

3001

BB9

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

GANTRY.PL.ERRFTHRESH

3001

Signed32

Read/Write

Position